I am having trouble building and running OpenSSH with Yocto for the LS1021A TWR board. The bitbake process seems to run fine, and the board boots. When the OpenSSH initialization starts and the key is generated, the key file cannot be written.
Starting OpenBSD Secure Shell server: sshd generating ssh RSA key... EXT2-fs (ram0): error: read_inode_bitmap: Cannot read inode bitmap - block_group = 34, inode_bitmap = 278530 Saving key "/etc/ssh/ssh_host_rsa_key" failed: Input/output error
It seems that /etc/ssh is mounted as read-only. For example:
root@ls1021atwr:/etc/ssh# touch file.txt
EXT2-fs (ram0): error: read_inode_bitmap: Cannot read inode bitmap - block_group = 34, inode_bitmap = 278530
touch: file.txt: Input/output error
I've tried adding OpsnSSH In my recipe a few different ways:
IMAGE_INSTALL += "packagegroup-core-ssh-openssh"
--OR--
CORE_IMAGE_EXTRA_INSTALL += " openssh"
CORE_IMAGE_EXTRA_INSTALL += " openssh-sftp"
CORE_IMAGE_EXTRA_INSTALL += " openssh-sftp-server"
Any ideas on how to get the folder writeable? Any workaround?
Thanks!
Hello Stuart Rubin,
I checked SDK 2.0 images on LS1021ATWR, there is no problem to create files in /etc/ssh folder.
Please check whether your Linux Kernel boot parameters is correct, please refer to the following.
root=/dev/ram rw console=ttyS0,115200 ramdisk_size=1000000
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------