Hi
I downloaded SDK 0.5 version, and compiled code, downloaded kernel.itb file to LS1043ARDB board, i connected a laptop to eth1 and assigned IP to eth1 ( now renamed as fm1-mac2 ), tried pinging, it displays network not reachable.
Am i missing anything here.
Thanks,
Manjunath
Note: I have attached logs generated from default image in RDB board and the image we build and executed.
Original Attachment has been moved to: Image_Build_log.zip
Original Attachment has been moved to: RDB_DefaultImage_Boot_log.zip
I am working at this problem. Please wait. You can also create service request for this problem to NXP technical support:
How to submit a new question for NXP Support
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Could you send dump for your current routing table.
Type the following command to display routing table:
# route
OR
# route -n
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Look at attached file. Test your board using similar command sequence:
ifconfig eth0 IP_address of your board.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
Thanks for reply, we did following steps
1) login as root
2) ifconfig fm1-mac2 169.254.140.233 ( With SDK 0.5 ethx as been renamed as fm1-macx )
3) ping 169.254.140.232 ( my laptop IP address )
it responds as
Network not reachable
Thanks,
Manjunath