NOR Booting in LS1043ARDB based custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NOR Booting in LS1043ARDB based custom board

726 Views
nikhilprakash
Contributor IV

Hi,

We are having an LS1043ARDB based custom board.We have flashed rcw,uboot,firmwares,file systems in bank 0 of fresh nor.Till uboot there is no issue.But on further booting kernel panic occurs.Is there any other thing we need to take care off for booting from fresh nor flash(any other firmwares or so).

Thanks in advance

Tags (2)
0 Kudos
2 Replies

616 Views
Pavel
NXP Employee
NXP Employee

Look at please the following page: https://community.freescale.com/message/634001?et=watches.email.thread#comment-634001

Draw attention about PPA microcode. You can disable this microcode or load this microcode3 to the NOR Flash.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

615 Views
nikhilprakash
Contributor IV

Hi Pavel,

We have tried this.Is there any other modifications needed.

Thanks

0 Kudos