Looking for boards with MPC7448, e.g. MCEVALHPC2-7448e

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Looking for boards with MPC7448, e.g. MCEVALHPC2-7448e

507 次查看
sverkernilsson
Contributor I

Hello,

We are looking for boards with the MPC7448 processor, for example in particular the evaluation board from NXP: MCEVALHPC2-7448e.

Does anybody know where to find such boards or have perhaps (even used units in good condition) some that we could get to buy?

We have specific requirements because the boards are going to be used for timing tests.

We would need about 6 units.

The specific requirements can be summarized as follows:

 

-          MPC7448 processor

-          Processor core clock 1.20 GHZ

-          Memory bus 133 MHZ

-          MPX bus 133 MHZ

-          Linux

I know I am sending this to the group for QorlQ processors, which may be a bit inappropriate as it is newer processors, but didn't find any group for older processors so I am trying this group if anybody has knowledge about legacy PowerPC processors.

Best regards,

Sverker Nilsson

0 项奖励
回复
1 回复

427 次查看
alexander_yakov
NXP Employee
NXP Employee

MPC7448 is mature product, and MCEVALHPC2-7448e board is not available for ordering anymore.

We do not sell used boards, sorry.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复