LSDK repos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK repos

1,252 Views
sp_qoriq
Contributor III

Any reason why the LSDK git repos are being moved?

For ex:

  Repo              previous git URL                                                                        new git URL

 ====               =============                                                                      ==========

mc-binary        https://github.com/qoriq-open-source/mc-binary                    https://github.com/NXP/qoriq-mc-binary.git

fman-ucode     https://github.com/qoriq-open-source/fm-ucode.git               https://github.com/NXP/qoriq-fm-ucode.git

 

Are there any plans to move other repos as well?

-Shiva

Tags (1)
0 Kudos
Reply
2 Replies

1,014 Views
sp_qoriq
Contributor III

Thanks for the reply, PavelChubakov‌. Agree that it doesn't affect the LSDK usage since these are mostly binary blobs with no custom board specific changes. But, are these plans to move other repos? If you move `uboot` or `linux` repos that could create problems for who mirroring these repos and adding our custom board specific changes in our own branches. 

0 Kudos
Reply

1,013 Views
Pavel
NXP Employee
NXP Employee

This changing does not produce any problem for LSDK using. New link shows that all files are in NXP folder. Perhaps it is a reason.
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply