LS1046 SGMII Clock - 100 vs 125MHZ serdes clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 SGMII Clock - 100 vs 125MHZ serdes clock

999件の閲覧回数
matthej
Contributor II

Hi,

 

We are using the SGMII interface at 1Gbps and have the choice of using a 125MHz or 100MHz SerDes clock to run these interfaces.

 

Right now, I have the clocks at 100MHz in my design. I was wondering if there is any performance differences between running at 100MHZ vs 125MHz in my design?

 

I could run both clocks in a different clock port I suppose and then run whichever I need to

 

Thanks!

0 件の賞賛
返信
2 返答(返信)

992件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could refer to LS1046ARDB to configure SERDES Reference Clocks as the following.

SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ

0 件の賞賛
返信

981件の閲覧回数
matthej
Contributor II

Thanks for your response.

 

My question is if I am using 3 SerDes lines for SGMII and I want to provide the LS1046 with both a 100MHz and 125MHZ which are valid clocks for this interface, how do I select which PLL to use to select the correct clock?

SD1_REF_CLK1: 100MHz

SD2_REF_CLK2: 125MHZ.

 

matthej_0-1626876969988.png

 

From the picture above it looks like I am able to select either REFCLK1 or REFLCK2 for PLL2 but only REFCLK1 for PLL1.

 

How do I select which PLL to use for this interface and am I correct in assuming that I am able to use either 100MHZ or 125MHZ clock for my current setup?

 

0 件の賞賛
返信