LS1043A JTAG Programming Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A JTAG Programming Connection

1,020件の閲覧回数
logeshs
Contributor II

Hi,

We are using LS1043A. I kindly request you to suggest us

1. what programmer should be used for programming LS1043A?

2. Programmer's operating Voltage level

3. Mating Connector part number of that programmer so that we can use it in our board.

4. Also if you have any datasheet for the programmer i request you to share the same to us.

Thanks.

0 件の賞賛
6 返答(返信)

790件の閲覧回数
ufedor
NXP Employee
NXP Employee

The request is not clear.

What exactly do you mean by "programming LS1043A"?

Which board is in question?

0 件の賞賛

790件の閲覧回数
logeshs
Contributor II

The question is about JTAG Configuration Signals Connector, Standard Cortex Debug Connector given in Figure.99 of LS1043A datasheet.

0 件の賞賛

790件の閲覧回数
ufedor
NXP Employee
NXP Employee

The header part number is Samtec FTSH-105-01-L-DV.

Other questions about "programmer" still are not clear.

Do you mean "debugger"?

If "yes", then refer to the following links:

CodeWarrior ARMv8 64 bit|NXP 

CodeWarrior TAP|NXP 

0 件の賞賛

790件の閲覧回数
logeshs
Contributor II

Yes, I mean about Debugger.

0 件の賞賛

790件の閲覧回数
logeshs
Contributor II

As per Figure.100 in LS1043A datasheet VDD is connected to 1.8V. Please confirm does the debugger supports/operates in 1.8V?

0 件の賞賛

790件の閲覧回数
ufedor
NXP Employee
NXP Employee

CoreWarrior TAP supports JTAG operation at 1.8V.

0 件の賞賛