LS1021A SPI NOR Flash Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A SPI NOR Flash Support

622件の閲覧回数
ramkrishnan
Contributor III

We are trying to figure out if we can attach a micron MT25QU512ABB spi flash to the LS1021A over the SPI (not the QSPI) and what files in the kernel and the uboot would need to be changed. I was trying to take a look to see if there is a template out there but the closest is the QSPI on the LS1021A IOT board. Could you point me in the right direction to get this working.

Thank you,

Ram Krishnan

タグ(3)
0 件の賞賛
1 返信

527件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Section 7.15.2.1 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

This Section contains information about dSPI using on the LS1021a boards.

 


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛