LS1020A starts not constantly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1020A starts not constantly

427 次查看
ilyaminaev
Contributor I

Hello. I created a motherboard with a 1020A processor. and when the board is turned on, the processor behaves differently each time. Often there are situations in which the processor does not respond to PORESET_B. This happens when the line RESET_REQ_B  produces 0. When   RESET_REQ_B  1 starts, the processor starts abnormally after PORESET_B, it is loaded from the SD card. But the processor starts randomly. What could be the problem of such impermanence?

0 项奖励
回复
1 回复

347 次查看
alexander_yakov
NXP Employee
NXP Employee

Please check if TRST pin is connected as recommended in LS1021A Design Checklist, Figure 32

LS1021A Design Checklist is available for download from LS1020A page, "Documentation" tab:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复