Hi, I use P1010 in my project. On the current evaluation board i have DDR3 1333 MHZ 9-9-9. but for our design we prefer 1066 Mhz 7-7-7 instead.
Will this be okay with this class of processor? Any way the processor seems to support maximum frequency of 800Mhz. Request an emergency reply.
Regards Ismail k k
解決済! 解決策の投稿を見る。
DDR3 1066MHz can operate using clock up to 533 MHz . A DDR3 RAM should operate down to 300 MHz (minimal clock frequency supported by DDR3 internal PLL) . Check the prefered DDR3 data sheet for the minimal supported clock frequency. If it supports 400 MHz then you can use it.
7-7-7-7 or 9-9-9-9 is question to the DDR3 hardware specs, I do not expect that DDR3 1066 noticably faster then DDR3 1333 at same clock of 400MHz.
DDR3 1066MHz can operate using clock up to 533 MHz . A DDR3 RAM should operate down to 300 MHz (minimal clock frequency supported by DDR3 internal PLL) . Check the prefered DDR3 data sheet for the minimal supported clock frequency. If it supports 400 MHz then you can use it.
7-7-7-7 or 9-9-9-9 is question to the DDR3 hardware specs, I do not expect that DDR3 1066 noticably faster then DDR3 1333 at same clock of 400MHz.
According with the P1010 Reference Manual, DDR memory controller operating a maximum 800 Mbps data rate (this means 400 MHz).
Adrian
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. QorIQ Processors ) to get it visible for active members.
For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )
Thank you for using Freescale Community.