How to read DCFG_CCSR_RSTRQPBLSR[ERR_CODE] register on ls1043 using codewarrior TAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to read DCFG_CCSR_RSTRQPBLSR[ERR_CODE] register on ls1043 using codewarrior TAP

564件の閲覧回数
benoitsansoni
Contributor II

Hi,

I am facing a problem with the RCW that I put on a QSPI flash.

Something goes wrong on RCW. The board is not booting.

In that way I decide to plug the codewarrior TAP to the board.

I just would like to read the dcfg_ccsr_rstrqpblsr[err_code] register to identify the cause of the RCW failure.

But when I try to establish a connection in that case with codewarrior, it is terminated and I am not able to establish a connection.

It works when I booted with other RCW.

How can I do to have a look on this register through the code warrior tap ?

Thanks

0 件の賞賛
1 返信

448件の閲覧回数
ufedor
NXP Employee
NXP Employee

Have you tried to Attach CodeWarrior - i.e. do not apply reset and execute an initialization script?

0 件の賞賛