How to read DCFG_CCSR_RSTRQPBLSR[ERR_CODE] register on ls1043 using codewarrior TAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to read DCFG_CCSR_RSTRQPBLSR[ERR_CODE] register on ls1043 using codewarrior TAP

567 Views
benoitsansoni
Contributor II

Hi,

I am facing a problem with the RCW that I put on a QSPI flash.

Something goes wrong on RCW. The board is not booting.

In that way I decide to plug the codewarrior TAP to the board.

I just would like to read the dcfg_ccsr_rstrqpblsr[err_code] register to identify the cause of the RCW failure.

But when I try to establish a connection in that case with codewarrior, it is terminated and I am not able to establish a connection.

It works when I booted with other RCW.

How can I do to have a look on this register through the code warrior tap ?

Thanks

0 Kudos
1 Reply

451 Views
ufedor
NXP Employee
NXP Employee

Have you tried to Attach CodeWarrior - i.e. do not apply reset and execute an initialization script?

0 Kudos