I am in Ubuntu. I am using SDK 1.7 document for reference.
What is the procedure to create a bootable SD/MMC-Card with U-boot for P2020RDB-PCA.?
We have used the following link for reference, but it is a different target - Orange Pi
Please suggest.
Thanks,
解決済! 解決策の投稿を見る。
This seems to be a typo.
In the document it is written:
"In SDK 1.6, after run “bitbake boot-format”, boot-format binary is deployed in <project>/tmp/sysroots/x86_64-linux/usr/bin/boot_format"
Please modify the command beginning:
# <install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format
as follows:
# <install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format/boot_format
Please note that it could be more convenient to put all three files (boot_format, U-Boot image and DAT file) into a single directory to simplify command sintax like:
./boot_format <config_file> <image> –sd <dev>
santosh@santosh-Inspiron-3542:~/Freescale/build/p2020rdb/tmp/sysroots/p2020rdb/usr/bin/boot_format $
~/Freescale/build/p2020rdb/tmp/sysroots/p2020rdb/usr/bin/boot_format ~/Freescale/build/p2020rdb/tmp/sysroots/p2020rdb/usr/share/boot_format/config_sram_p1022ds.dat u-boot-sd-P2020RDB-PC_SDCARD-2014.07+fslgit-r0.bin -sd /dev/mmcblk0
bash: /home/santosh/Freescale/build/p2020rdb/tmp/sysroots/p2020rdb/usr/bin/boot_format: Is a directory
This seems to be a typo.
In the document it is written:
"In SDK 1.6, after run “bitbake boot-format”, boot-format binary is deployed in <project>/tmp/sysroots/x86_64-linux/usr/bin/boot_format"
Please modify the command beginning:
# <install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format
as follows:
# <install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format/boot_format
Please note that it could be more convenient to put all three files (boot_format, U-Boot image and DAT file) into a single directory to simplify command sintax like:
./boot_format <config_file> <image> –sd <dev>
'<install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format' is a directory.
'<install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format'
This obviously is an example which can't be used "as is".
Note that <install_path> represents a placeholder for the real PATH string.
It is a software developer responsibility to adjust the command for the specific case.
We used the real PATH, I did not place it 'as is'. I am doubtful if the command syntax is correct as the first argument we are giving a directory path without any file
Excuse me, it was several times requested to provide REAL command string and log.
The steps that we did after inserting a blank 4GB SD card into the Linux Host are as follow:
# fdisk /dev/mmcblk0 (This command is used to divide the card into two partitions, one for fat16 file system(1GB) and another for ext4 file system(3GB))
The current partitions that are configured on the host are as follow:
Disk /dev/mmcblk0: 4026 MB, 4026531840 bytes
4 heads, 16 sectors/track, 122880 cylinders, total 7864320 sectors
Units = sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x08836c9a
Device Boot Start End Blocks Id System
/dev/mmcblk0p1 2048 2099199 1048576 e W95 FAT16 (LBA)
/dev/mmcblk0p2 2099200 7864319 2882560 83 Linux
After this partitioning the following command need to be executed I suppose:
<path>/boot_format <config_file> <image> -sd <dev>
The above command expands as follow:
# <install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format <install_path>/build_p1020rdb_release/ tmp/sysroots/x86_64-linux/share/boot_format/config_sram_p2020rdb.dat u-boot-sd-P2020RDB-PC_SDCARD.bin -sd /dev/mmcblk0
The above command seem to be copying config file and bin file to sd/mmc card.
But this command is not working.
Please provide the commad execution log.
Thanks for the reply.
Can you explain the command:
# <install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format <install_path>/build_p1020rdb_release/ tmp/sysroots/x86_64-linux/share/boot_format/config_sram_p1022ds.dat u-boot-sd-P2020RDB-PC_SDCARD.bin -sd /dev/sdb
We tried with it, it says '<install_path>/build_p1020rdb_release/tmp/sysroots/x86_64-linux/usr/bin/boot_format' is a directory.
What exactly you have tried?
Please provide the log.