How to configure JTAG chain for a DDR validation connection?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure JTAG chain for a DDR validation connection?

506 Views
tiagobrusamarel
Contributor V

Hello,

I'm trying to figure out how to configure the JTAG chain in a DDR validation connection as I already do for the debug connection. Can anyone help me?

0 Kudos
Reply
1 Reply

374 Views
ufedor
NXP Employee
NXP Employee

For running DDR validation on a target with multiple devices in the JTAG chain,
two files have to be modified. Modifications are provided in attached files
(look for the comment "# Workaround for complex JTAG chain").

These files are located in:
\CW_PA_v10.5.1\eclipse\Optimization\resources\QorIQ\common\templates\init\

Eclipse/CW must be restarted to use modified files.

0 Kudos
Reply