How to add the Serial Library to a project with CPC as SRAM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add the Serial Library to a project with CPC as SRAM?

ソリューションへジャンプ
1,994件の閲覧回数
hymalaibello
Contributor III

Hi! It works! thank you very much! Now I would like to use only CPC as SRAM, but the build configuration of Downloads_SRAM does not include the libraries for Serial communication (Printf). I want to know if  there is a way to include them?, because I need to send the data using Serial Port.

Thanks!

Regards,

Hymalai Bello

1 解決策
1,774件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hymalai,

SRAM CodeWarrior project doesn't include "printf" to make the debugged ELF file smaller, because CPC or L2 to SRAM is always in a small size. P4080DS CPC to SRAM  is 1M, it could accommodate the ELF(with printf) and performing debug.


Please try to use the following method.

Please follow the bare board project wizards to create a "Download" project(RAM version), then change the lcf file as "e500mc_gcc-eabi_SRAM.lcf" from Project->Properties->C/C++ Build->Settings->PowerPC EABI e500mc C Linker->PowerPC Environment.

Please remember to change the initialization file as SRAM version "P4080DS_init_sram.tcl"  from Run->Debug Configurations->Edit->Edit->Initialization->Initialize target script.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,775件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Hymalai,

SRAM CodeWarrior project doesn't include "printf" to make the debugged ELF file smaller, because CPC or L2 to SRAM is always in a small size. P4080DS CPC to SRAM  is 1M, it could accommodate the ELF(with printf) and performing debug.


Please try to use the following method.

Please follow the bare board project wizards to create a "Download" project(RAM version), then change the lcf file as "e500mc_gcc-eabi_SRAM.lcf" from Project->Properties->C/C++ Build->Settings->PowerPC EABI e500mc C Linker->PowerPC Environment.

Please remember to change the initialization file as SRAM version "P4080DS_init_sram.tcl"  from Run->Debug Configurations->Edit->Edit->Initialization->Initialize target script.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------