FRWY-LS1046A-AC DDR4配置咨询

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRWY-LS1046A-AC DDR4配置咨询

ソリューションへジャンプ
1,624件の閲覧回数
tian_shuliang
Contributor I

想确认下:

 

1.使用FRWY-LS1046A-AC单板的代码是否可以兼容DDR4(MT40A1G16RC-062E芯片?如果兼容,DDR4是否有降频的可能?

2.如果不兼容,是否有DDR4(MT40A1G16RC-062E)时序配置的相关patch?

3.如果没有patch,确认下是否只修改参数ddr_raw_timing(路径:packages/firmware/atf/plat/nxp/soc-ls1046/ls1046afrwy/ddr_init.c)即可?

0 件の賞賛
返信
1 解決策
1,352件の閲覧回数
Bulat
NXP Employee
NXP Employee

Please use English for future communications in NXP Community.

1,2. The LS1046A supports DDR4 only. So yes, it is compatible with DDR4 in general and with MT40A1G16RC-062E in particular.

3. Yes, you can modify ddr_raw_timing in accordance with the new memory parameters.

Regards,

Bulat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,352件の閲覧回数
tian_shuliang
Contributor I

@Bulat Karymov  OK,thanks。

0 件の賞賛
返信
1,353件の閲覧回数
Bulat
NXP Employee
NXP Employee

Please use English for future communications in NXP Community.

1,2. The LS1046A supports DDR4 only. So yes, it is compatible with DDR4 in general and with MT40A1G16RC-062E in particular.

3. Yes, you can modify ddr_raw_timing in accordance with the new memory parameters.

Regards,

Bulat

0 件の賞賛
返信