FRDM-LS1012A Board Qspi nor Quad mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-LS1012A Board Qspi nor Quad mode

751 Views
beanhuo
Contributor I

hi, 

we purchased one FRDM-LS1021A board, want to de-solder onboard current Qspi nor, and re-solder one Micron Qspi nor with Quad mode. From your document and schematic said that this board only can support X1 or X2 mode.

does this mean that your PCB layout isn't for X4?

0 Kudos
Reply
2 Replies

584 Views
ghislainprovost
Contributor I

Hi Pavel,

I would like to modify this design for having the 4 bit routed? I observed the signal PROC_RESET_REQ_B, which is the 4th QSPI bit,  is used to reset the board. Can you describe when is this signal asserted? 

Ghislain

0 Kudos
Reply

584 Views
Pavel
NXP Employee
NXP Employee

Yes, the FRDM-LS1012A layout uses only two data lines of the LS1012a QSPI. See attached screenshot of the FRDM-LS1012A schematic:

http://www.nxp.com/downloads/en/printed-circuit-boards/FRDM-1012A-PA-DF.zip


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply