Before I start - Yes, I have googled and read many posts about this issue, but I did
not find an article that answers posed kin this post
-----------------
Hi,
I have professional version of CodeWarrior (Development Studio for QorIQ) connect to a
Custom LS1043A-RGW via a CodeWarrior Tap (brand new). I have the Software Switches
set to boot from SD Card (and I have an SD Card that apparently has proper RCW settings
written (I will be asking a question about this later))
I am using default <xxxx>\ARMV8\gdb\bin\aarch64-fsl-gdb.exe for debug and
have successfully debugged some programs (see below), but while try to run a
simple DDR-based bare-metal application and I get:
Error in final launch sequence
Failed to execute MI command:
load C:\\Users\\xxxxx\\eclipse-workspace\\b4\\Debug\\b4.elf
Error message from debugger back end:
Load failed
Load failed
Here are the steps to re-create.
QCVS DDR source output
-----
Attached is the diagnostic info (including a picture of this posting along with the Error in Codewarrior screen)
Since your DDR initialization settings were tested using OCRAM project, CodeWarrior should correctly load code to DDR on your board.
Do you change DDR initialization settings in the .tcc on your DDR initialization settings?
Is there problem for code loading using this .tcc file on your board?
Have a great day,
Pavel Chubakov
CodeWarrior uses .TCC file for board configuring before code loading.
See the Chapter 5 in the ARMv8_Targeting_Manual.pdf file. This file is available using the following path:
C:\Freescale\CW4NET_v2019.01\CW_ARMv8\ARMv8\Help\PDF
The init_DDRC() should be added to active .tcc file.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------