Docbook utils build issue with QorIQ Linux SDK 2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Docbook utils build issue with QorIQ Linux SDK 2.0

659 次查看
sarayuksivanand
Contributor I

Hi all ,

I am trying to build the QorIQ Linux SDK 2.0 on my ubuntu setup and i am seeing some strange issue with the docbook-utils . Can you please help me with the same.

Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4
| Making all in backends
| make[1]: Entering directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/backends'
| make[1]: Nothing to be done for 'all'.
| make[1]: Leaving directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/backends'
| Making all in bin
| make[1]: Entering directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/bin'
| make[1]: Nothing to be done for 'all'.
| make[1]: Leaving directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/bin'
| Making all in doc
| make[1]: Entering directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc'
| Making all in refentry
| make[2]: Entering directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc/refentry'
| make[2]: Nothing to be done for 'all'.
| make[2]: Leaving directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc/refentry'
| Making all in man
| make[2]: Entering directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc/man'
| make[2]: Nothing to be done for 'all'.
| make[2]: Leaving directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc/man'
| Making all in HTML
| make[2]: Entering directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc/HTML'
| SGML_CATALOG_FILES=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/x86_64-linux/etc/sgml/catalog \
| SGML_SEARCH_PATH=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14:/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc:.. \
|     jade -t sgml -i html -d /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/docbook-utils.dsl\#html \
|         -V '%use-id-as-filename%' /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc/docbook-utils.sgml
| SGML_CATALOG_FILES=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/x86_64-linux/etc/sgml/catalog \
| SGML_SEARCH_PATH=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14:/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc:.. \
|     jade -t sgml -i html -d /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/docbook-utils.dsl\#html \
|         -V '%use-id-as-filename%' /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc/docbook-utils.sgml
| SGML_CATALOG_FILES=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/x86_64-linux/etc/sgml/catalog \
| SGML_SEARCH_PATH=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14:/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc:.. \
|     jade -t sgml -i html -d /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/docbook-utils.dsl\#html \
|         -V '%use-id-as-filename%' /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc/docbook-utils.sgml
| SGML_CATALOG_FILES=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/x86_64-linux/etc/sgml/catalog \
| SGML_SEARCH_PATH=/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14:/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc:.. \
|     jade -t sgml -i html -d /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/docbook-utils.dsl\#html \
|         -V '%use-id-as-filename%' /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/docbook-utils-0.6.14/doc/docbook-utils.sgml
| Makefile:458: recipe for target 'docbook2man.html' failed
| make[2]: *** [docbook2man.html] Segmentation fault (core dumped)
| make[2]: *** Waiting for unfinished jobs....
| Makefile:458: recipe for target 'api.html' failed
| make[2]: *** [api.html] Segmentation fault (core dumped)
| Makefile:458: recipe for target 'docbook2texi.html' failed
| make[2]: *** [docbook2texi.html] Segmentation fault (core dumped)
| Makefile:458: recipe for target 'backend-spec.html' failed
| make[2]: *** [backend-spec.html] Segmentation fault (core dumped)
| make[2]: Leaving directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc/HTML'
| Makefile:298: recipe for target 'all-recursive' failed
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory '/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/build/doc'
| Makefile:379: recipe for target 'all-recursive' failed
| make: *** [all-recursive] Error 1
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/x86_64-linux/docbook-utils-native/0.6.14-r3/temp/log.do_compile.20775)
ERROR: Task 6 (/home/sarayu/code/yocto_arm/QorIQ-SDK-V2.0-20160527-yocto/sources/poky/meta/recipes-devtools/docbook-utils/docbook-utils-native_0.6.14.bb, do_compile) failed with exit code '1'

0 项奖励
1 回复

464 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello sarayu k sivanandam,

I use Ubuntu 14.04, didn't find this problem when building docbook-utils-native.

Please install the following packages on your host machine.

$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm

Extra packages are needed for Ubuntu-64b:
$ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 ia32-libs lib32ncurses5-dev


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励