Do the interfaces in the b4860qds support multicast?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do the interfaces in the b4860qds support multicast?

598件の閲覧回数
victorgomez
Contributor II

Hi There!

I am running into problems when using multicast in two different b4860qds boards Do these boards support multicast at all?

Thanks!

0 件の賞賛
返信
1 返信

554件の閲覧回数
bpe
NXP Employee
NXP Employee

Yes, multicast is supported by DPAA, there are no known issues with hardware or software:

Submit Form


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信