CodeWarrior for Power Architecture 8.8 - which processor family for P1020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior for Power Architecture 8.8 - which processor family for P1020

634 次查看
larryharmon
Contributor II

I have installed an evaluation version of CodeWarrior for windows.

I have a P1020WLAN development system with an e500 processor, which is not in CodeWarrior's list of supported families.

Which processor family should I select to support the P1020WLAN kit?

0 项奖励
1 回复

438 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

Neither CW Classic nor CW Eclipse supports P1020WLAN.

I suggest to use any board that has a P1020 processor (as far I know for CW 8.8 there is a P1020 Service Pack that you can install) and to select the SRAM cfg file instead the default core cfg file (this way because the core cfg file contains the DRAM board specific settings and I'm pretty sure that will not work with your WLAN board.) 

Secondly, please update the stack and the heap address (from project properties) to fit in the SRAM area (you'll need this update if you need to make a download debug, if not just use the Connect target - Flash Programmer usage for example is enough).

Regards,

Marius

0 项奖励