Can LS1046A and LS1026A share Same Openwrt source cord?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can LS1046A and LS1026A share Same Openwrt source cord?

809 次查看
ken_jung
Contributor I

Can LS1046A and LS1026A share Same Openwrt source cord?

0 项奖励
回复
1 回复

697 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, both devices are based on the same silicon, the difference is only in number of cores (LS1026A has 2 cores instead of 4), so the software designed for LS1046A will work on LS1026A with very little or no modifications.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复