Can I have sample of elf file but not uboot which I can try to load on t2080e SDK taget, thanks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I have sample of elf file but not uboot which I can try to load on t2080e SDK taget, thanks

跳至解决方案
2,144 次查看
sergeyuskach
Contributor I

Hi,

I am bringing up  new development envoro0nment for t2080e SDK board and what eevr files was shipped with this board are binary. Can I have a copy of ELF files for Linux so I can laod this elf file using emulator.

Thanks

0 项奖励
回复
1 解答
1,982 次查看
addiyi
NXP Employee
NXP Employee

vmlinux is built with debug symbols, from SDK 1.8.

Adrian

在原帖中查看解决方案

0 项奖励
回复
11 回复数
1,981 次查看
addiyi
NXP Employee
NXP Employee

You can take the SDK sources from Freescale site and build the images by yourself and you will have the elf file.

Adrian

0 项奖励
回复
1,981 次查看
sergeyuskach
Contributor I

Hi Adrian:

thanks for a reply , I can do it but my development environment is Windows or Cigwin, can you build it using Cigwin ?

Can you point me to how to build document.

Thanks

0 项奖励
回复
1,981 次查看
addiyi
NXP Employee
NXP Employee

No sure about building using cygwin. But, why don't you used a linux virtual machine?

Adrian

0 项奖励
回复
1,982 次查看
sergeyuskach
Contributor I

Hi Adrian:

I do not have one. If I have one I would not ask you this questions

Thanks

0 项奖励
回复
1,982 次查看
addiyi
NXP Employee
NXP Employee

You have to build the images from sources, to have sync between elf and bin files.

Adrian

0 项奖励
回复
1,982 次查看
sergeyuskach
Contributor I

Hi Adrian:

It looks like I am asking you for something to help me with and you are trying to dodge it.

Can you just give me vmlinux.elf file. I do not need any source and I cannot build it.

Is it too difficult ?

Thanks

0 项奖励
回复
1,982 次查看
addiyi
NXP Employee
NXP Employee

It is not difficult, but I don't know the options used for building kernel image in SDK, this is way the recommendation is to build the kernel by yourself.

Adrian

0 项奖励
回复
1,982 次查看
sergeyuskach
Contributor I

Hi Adrain:

It looks like blind person trying to talk to mute one.

Can you send me any vmlinux.elf build to the eval board I have , I keep repeating that I do not have linux machine to build and each time you are ignoring it.

Is my English is so bad that you could not understand it ?

Thanks

0 项奖励
回复
1,982 次查看
addiyi
NXP Employee
NXP Employee

What target you need to have built (t2080qds-64b, t2080qds, t2080rdb-64b, t2080rdb) and what SDK version?

0 项奖励
回复
1,982 次查看
sergeyuskach
Contributor I

t2080qds-64b any version , I just need elf file

0 项奖励
回复
1,983 次查看
addiyi
NXP Employee
NXP Employee

vmlinux is built with debug symbols, from SDK 1.8.

Adrian

0 项奖励
回复