I am trying to run a simple “Hello World!” program on the NXP P2041RDB-PC DEV BRD. I need to write this program in C++, but I am not sure what compiler to use so that it will run on the board. I am new to this type of environment so I am just trying to develop and run a program on the board for starters. Any help or pointers to any other resources would be greatly appreciated. Thank you!
已解决! 转到解答。
Adrian,
I made a make file and it looks like this
-------------------------------------------------
####
SDKTARGETSYSROOT = /opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/ppce500mc-fsl_networking-linux
CROSS_COMPILE = /opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/bin/ppce500mc-fsl_networking-linux/powerpc-fsl_networking-linux-
CC = $(CROSS_COMPILE)gcc -m32 -msoft-float -mcpu=e500mc --sysroot=${SDKTARGETSYSROOT}
LD = $(CROSS_COMPILE)ld
SOURCES = main.o
BIN = test
all:
$(CC) -o main.o -c main.c
$(CC) -o $(BIN) $(SOURCES)
clean:
rm -f $(BIN) ./$(BIN) ${SOURCES}
####
-------------------------------------------------
The make file works fine and produces the test executable file.
The issue still arises that the P2041RDB-PC DEV BOARD "can not execute the binary file"
I have checked the file size after moving it to check the integrity and it doesn't look like it is being changed any during the transfer using the USB device at all.
I am not sure what I should be doing to write a program and have the P2041RDB-PC DEV BOARD execute it.
I am trying to execute it with bash test on the board.
Is there something that I am doing wrong or missing? I have followed every example and test I can find and nothing seems to be working.
Thank you,
Isaac
I was finally able to have the p2041 execute a program Adrian! Thank you so much for your help! It looks like the type of file system being used by the USB to transfer was causing permission issues with the contents it contained when dealing with the p2041, relating to the most recent issue that we talked about above. Thanks again!
Here is an example of makefile using sdk standalone toolchain. This is not for your toolchain, but you can use it as example. Also, note that SDK toolchain is a sysrooted toolchain. It means that toolchain will start to look for target fragments and libraries starting from the path specified by the sysroot option.
####
SDKTARGETSYSROOT = /opt/fsl-networking/QorIQ-SDK-V1.7-MPC832XMDS/sysroots/ppce300c2-fsl-linux
CROSS_COMPILE = /opt/fsl-networking/QorIQ-SDK-V1.7-MPC832XMDS/sysroots/x86_64-fslsdk-linux/usr/bin/powerpc-fsl-linux/powerpc-fsl-linux-
CC = $(CROSS_COMPILE)gcc -m32 -msoft-float -mcpu=e300c2 --sysroot=${SDKTARGETSYSROOT}
LD = $(CROSS_COMPILE)ld
SOURCES = main.o
BIN = test
all:
$(CC) -o main.o -c main.c
$(CC) -o $(BIN) $(SOURCES)
clean:
rm -f $(BIN) ./$(BIN) ${SOURCES}
###
Adrian
Adrain,
I am having an issue with the board not executing the compiled a.out file.
Here is step by step what I did
-----------------------------------------------------------------------------------------------------------------
cyber@cyber-Latitude-E6510:~$ cd /opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ ls
a.out as cc1plus cpp ld liblto_plugin.so liblto_plugin.so.0.0.0 lto-wrapper objcopy plugin strip
ar cc1 collect2 gcc liblto_plugin.la liblto_plugin.so.0 lto1 nm objdump ranlib
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ cat /home/cyber/Desktop/C_helloWorldProgram.c
//C hello world example
#include <stdio.h>
int main()
{
printf("Hello world\n");
return 0;
}
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ sudo /opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2/gcc /home/cyber/Desktop/C_helloWorldProgram.c
[sudo] password for cyber:
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ ls
a.out as cc1plus cpp ld liblto_plugin.so liblto_plugin.so.0.0.0 lto-wrapper objcopy plugin strip
ar cc1 collect2 gcc liblto_plugin.la liblto_plugin.so.0 lto1 nm objdump ranlib
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ file a.out
a.out: ELF 32-bit MSB executable, PowerPC or cisco 4500, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.16, BuildID[sha1]=0x86aff26ce396f3dfc3665dd5311a997648fe03d6, not stripped
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$
THE A.OUT IS NOW DONE
powerpc-fsl_networking-linux/4.7.2
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ ls
a.out as cc1plus cpp ld liblto_plugin.so liblto_plugin.so.0.0.0 lto-wrapper objcopy plugin strip
ar cc1 collect2 gcc liblto_plugin.la liblto_plugin.so.0 lto1 nm objdump ranlib
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ sudo mv a.out /media/NTFS_USB
cyber@cyber-Latitude-E6510:/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2$ cd /media/NTFS_USB
cyber@cyber-Latitude-E6510:/media/NTFS_USB$ ls
a.out
THE A.OUT IS ON A USB DRIVE
Welcome to minicom 2.5
OPTIONS: I18n
Compiled on May 2 2011, 10:05:24.
Port /dev/ttyUSB0
Press CTRL-A Z for help on special keys
Poky 9.0 (Yocto Project 1.4 Reference Distro) 1.4 p2041rdb ttyS0
p2041rdb login: AT S7=45 S0=0 L1 V1 X4 &c1 E1 Q0
p2041rdb login: root
root@p2041rdb:~# ls
root@p2041rdb:~#
CONNECTED TO THE P2041RDB-PC
root@p2041rdb:~# cd /media
root@p2041rdb:/media# ls
card hdd net realroot sda3 union
cf mmc1 ram sda1 sdb1
root@p2041rdb:/media# cd sdb1
root@p2041rdb:/media/sdb1# ls
a.out
root@p2041rdb:/media/sdb1# bash ./a.out
./a.out: ./a.out: cannot execute binary file
root@p2041rdb:/media/sdb1# ./a.out
-sh: ./a.out: Permission denied
I TRY TO RUN THE PROGRAM FROM THE USB AND IT WILL NOT WORK
root@p2041rdb:/media/sdb1# mv a.out /home
mv: can't remove 'a.out': Read-only file system
root@p2041rdb:/media/sdb1# ls
a.out
I TRY TO MOVE IT AND THEN IT FAILS TO MOVE
root@p2041rdb:/media/sdb1# ls
a.out
root@p2041rdb:/media/sdb1# cd /home
root@p2041rdb:/home# ls
a.out root
root@p2041rdb:/home# ./a.out
-sh: ./a.out: Permission denied
root@p2041rdb:/home# bash ./a.out
./a.out: ./a.out: cannot execute binary file
BUT SOMEHOW THE MOVE DOES WORK, EVEN THOUGH IT GIVES A READ-ONLY FILE SYSTEM ERROR. IT FAILS TO RUN THOUGH STILL.
----------------------------------------------------------------------------------
I have no idea what I am doing wrong. Do you have any idea why I can not get the p2041rdb to execute any code at all?
Thank you for your time,
Isaac
Go to www.nxp.com/infocenter/ > Software and Tools > QorIQ > SDK > QorIQ SDK 1.9 Documentation > Getting Started with Yocto Project > Additional Instruction for Developers > Installing the Toolchain to find out how to install the the standalone toolchain.
Adrian
Hi Adrian,
I was able to install the
~/QorIQ-SDK-V1.4-20130625-yocto/build_p2041rdb_release
and also
/opt/fsl-networking/QorIQ-SDK-V1.4/sysroots/x86_64-fsl_networking_sdk-linux/usr/libexec/ppce500mc-fsl_networking-linux/gcc/powerpc-fsl_networking-linux/4.7.2
after the first part.
In the 4.7.2 directory there is a gcc program. If I compile a C program(not C++) with gcc, and move that program to an USB drive and move the program from the USB drive onto the drive on the pP2041, should the program run when executed?
Also, is cpp another C compiler and linker or would C++ work with the cpp program?
Thank you for the help,
Isaac