About UART operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About UART operation

324件の閲覧回数
kojimiura
Contributor I
UART2_SIN is pulled down with 10kΩ.
When not using UART2 (DUART registers remain at their initial values)
1. Will it harm my device?
2. Would you like to receive data?
3. Is it possible for the CPU to be interrupted for some reason?
4. Is it okay if the Divisor setting value is zero?
Thank you.
0 件の賞賛
返信
6 返答(返信)

240件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

When not using UART2 , the response for the above-stated queries are as follows:
1. Will it harm my device
No

2. Would you like to receive data?
No

3. Is it possible for the CPU to be interrupted for some reason?
No

4. Is it okay if the Divisor setting value is zero?
Does not matter.

0 件の賞賛
返信

285件の閲覧回数
kojimiura
Contributor I

What do you think after that?

0 件の賞賛
返信

280件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 件の賞賛
返信

184件の閲覧回数
kojimiura
Contributor I

Since the internal clock of UART2 is disabled, Start bit is not detected. Is this understanding correct?

0 件の賞賛
返信

177件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

0 件の賞賛
返信

174件の閲覧回数
kojimiura
Contributor I
Thank you.
0 件の賞賛
返信