About UART operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About UART operation

552 次查看
kojimiura
Contributor I
UART2_SIN is pulled down with 10kΩ.
When not using UART2 (DUART registers remain at their initial values)
1. Will it harm my device?
2. Would you like to receive data?
3. Is it possible for the CPU to be interrupted for some reason?
4. Is it okay if the Divisor setting value is zero?
Thank you.
0 项奖励
回复
6 回复数

468 次查看
yipingwang
NXP TechSupport
NXP TechSupport

When not using UART2 , the response for the above-stated queries are as follows:
1. Will it harm my device
No

2. Would you like to receive data?
No

3. Is it possible for the CPU to be interrupted for some reason?
No

4. Is it okay if the Divisor setting value is zero?
Does not matter.

0 项奖励
回复

513 次查看
kojimiura
Contributor I

What do you think after that?

0 项奖励
回复

508 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 项奖励
回复

412 次查看
kojimiura
Contributor I

Since the internal clock of UART2 is disabled, Start bit is not detected. Is this understanding correct?

0 项奖励
回复

405 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

0 项奖励
回复

402 次查看
kojimiura
Contributor I
Thank you.
0 项奖励
回复