在PPC环境安装SDK2.0时总是报错Error: Unsupported Distribution, Exit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

在PPC环境安装SDK2.0时总是报错Error: Unsupported Distribution, Exit

947件の閲覧回数
魏传奇
Contributor I

在PPC环境安装SDK2.0时总是报错

root@t1040d4rdb:~# cd QorIQ-SDK-V2.0-20160527-yocto/
root@t1040d4rdb:~/QorIQ-SDK-V2.0-20160527-yocto# ./sources/meta-freescale/scripts/host-prepare.sh

Error: Unsupported Distribution, Exit

如何解决?谢谢

0 件の賞賛
1 返信

572件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use Ubuntu 14.04 for this SDK.

Look at the Section 3.2.2 of SDK 2.0-1703 documentation about SDK 2.0 installing:

http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛