Loading DSP using IPC on B4860QDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loading DSP using IPC on B4860QDS

1,409 Views
andrewmarles
Contributor I

I am having an issue loading code on the B4860QDS platform.  This is using the most recent 2.0 SDK as well as with 1.9.  The application I am loading is the ipc_integration demo from the SmartDSP examples.  I have converted the bin using sc100-elf2xx.exe. dsp_bt fails with the following error:

root@b4860:/ipc# ./dsp_bt -h 0 -c 0 -i c0_ipc_demo_b4860_dbg.bin
===B4860QDS DSP boot Application (3.1.0) ===
SYSTEM MAP
DSP PrivArea: Addr=80000000 Size=7ff00000
Shared CtrlArea: Addr=fff00000 Size=100000
DSP Core0 M2: Addr=0 Size=0
DSP Core1 M2: Addr=0 Size=0
DSP M3: Addr=c40000000 Size=8000
PA CCSRBAR: Addr =ffe000000 Size=1000000
DSP CCSRBAR: Addr =ffe000000 Size=1000000
PA Shared Area: Addr=50000000 Size=f000000
DSP Shared Area: Addr=5f000000 Size=1000000
Waiting for FI
Waiting for FI
Waiting for FI
L2 cache cluster2 init
Loading Dsp image c0_ipc_demo_b4860_dbg.bin

Error in mapping physical address 100000000 to virtual address in load_dsp_image
Error in loading Dsp image StarCore

I have re-compiled the kernel as indicated in the SDK documentation, but the error persists.  I have found somewhat similar issues discussed elsewhere.

Is there a current SDK example with a known good configuration to demonstrate IPC functionality?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,056 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Andrew Marles,

It seems that there is problem in the memory allocation, please check whether you missed some steps as the following.

u-boot bootargs:

=>setenv bootm_size 0x70000000

=>setenv bootargs 'console=ttyS0,115200 default_hugepagesz=256m hugepagesz=256m hugepages=1'

cd /usr/driver/IPC/single_rat/
echo 0x10000000 > /proc/sys/kernel/shmmax
insmod hetmgr.ko
insmod shm.ko
insmod l1d.ko
mknod /dev/fsl_l1d c 249 0
mknod /dev/fsl_shm c 250 0
mknod /dev/het_mgr c 251 0


# ./dsp_bt -h 1 -c 0 -i c0.bin -c 1 -i c1.bin

# ./ipc_test -r 0 -i 10

In addition, please refer to the following Kernel build option.

1. Diable the Kernel dma engine

Device Drivers  --->
 [ ] DMA Engine support  --->

2. Enable Userspace's I/O driver

Device Drivers  --->
 <*> Userspace I/O drivers  --->
  <*> Freescale DMA support

3. Build below packages into rootfs

NOTE: fsl-image-core.bb

IMAGE_INSTALL += " \

    ipc-ust \
    ipc-modules-single \
    ipc-modules-multi \
"

If your problem persists, please attach your whole console log.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply