Hi,Yiping.recently I met a problem.
My board is P4080ds,I want to test the lpm-ipfwd demo.I configured the fm1-gb2 and fm2-gb3 as share-mac, and when I ran the lpm-ipfwd demo,at the beginning of about 3 hours,it worked well.But after 3 hours,promblem happened.The fm2-gb3 ping time out,but the fm1-gb2 ping well.I typed "ps -A | grep lpm_ipfwd_app",it still there:" 1655 ttyS0 lpm_ipfwd_app". It looks like that lpm_ipfwd_app was still working,but fm2-gb3 cannot work,so how could I solve the problem?
appendix:
the command is :lpm_ipfwd_app 1..7 -c usdpaa_config_p4_serdes_0xe.xml -p usdpaa_policy_hash_ipv4_arp_coarse_classify.xml -d 0x10000000 -b 1600:1600:1600 -n.
解決済! 解決策の投稿を見る。
Hello Feifei,
In your original description, you pass the serdes 0xe configuration file to fmc, it seems that this is not coincident with your current target configuration.
Would you please also provide u-boot and Kernel log? It's better to include steps to setup lpm_ipfwd_app.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Feifei,
Would you please provide the console log for running lpm_ipfwd_app? Probably the system provide some error information for debugging.
Thanks,
Yiping
Hi,Yiping,
there was no error information in the console log.
Yestoday,I did an experiment :I unplugged the Ethernet cable which connected to Internet,with only a local area network left.The lpm-ipfwd demo ran well all the time,and the fm1-gb2 and fm2-gb3 ping well.
But about 3 hours after I using the Ethernet cable to connect the Internet,promblem happened,The fm2-gb3 ping time out,but the fm1-gb2 ping well.I typed "ps -A | grep lpm_ipfwd_app",it still there:" 1655 ttyS0 lpm_ipfwd_app". It looks like that lpm_ipfwd_app was still working,but fm2-gb3 cannot work.(fm1-gb2 acess to LAN and fm2-gb3 acess to Internet)
I typed the following command:
root@p4080ds:~# ifconfig fm2-gb3
fm2-gb3 Link encap:Ethernet HWaddr 00:0c:bd:00:d0:95
inet addr:192.168.2.221 Bcast:192.168.2.255 Mask:255.255.255.0
inet6 addr: fe80::20c:bdff:fe00:d095/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:1305442 errors:0 dropped:941 overruns:0 frame:0
TX packets:23140 errors:1220 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:146255111 (139.4 MiB) TX bytes:3570626 (3.4 MiB)
Memory:fe5e6000-fe5e6fff
Then I referred to the document Data Path Acceleration Architecture Debug(FTF-NET-F0148),and I typed some command as follows to check that if fm2-gb3 could receive frames:
root@p4080ds:~# ls /sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/*
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_dealloc_buf
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_discard_frame
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_enq_total
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_frame
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_rx_bad_frame
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_rx_filter_frame
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_rx_large_frame
/sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/port_rx_out_of_buffers_discard
root@p4080ds:~# cat /sys/devices/ffe000000.soc/ffe500000.fman/ffe58b000.port/statistics/*
fm1-port-rx3 counter: 0
fm1-port-rx3 counter: 0
fm1-port-rx3 counter: 1337585
fm1-port-rx3 counter: 1800718
fm1-port-rx3 counter: 0
fm1-port-rx3 counter: 0
fm1-port-rx3 counter: 0
fm1-port-rx3 counter: 463133
It shows that the count of port_rx_out_of_buffers_discard is 463133,and the counts of port_rx_out_of_buffers_discard is always incremented.
The document shows that the defination of port_rx_out_of_buffers_discard is that
Number of received frames that were discarded due to lack of external buffers.
Counts the number of frames on the Rx port that were not able to enter the receive queue, since buffer allocation has failed.
It looks like that once I used the Ethernet cable to connect the Internet, problem happened,and the buffers is not enough,so how could I solve the problem?
Hello Feifei,
In P4080DS default shared MAC device tree p4080ds-usdpaa-shared-interfaces.dts, fm2-10g is defined as the shared MAC interface between USDPAA and Linux.
In your description, you mentioned that you configured fm1-gb2 and fm2-gb3 as shared MAC interfaces between USDPAA and Linux. How do you modify the shared MAC device tree to define these two shared MAC interfaces? How do you define the buffer pools and QMAN tx and rx frame queues in your modified dts file?
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,Yiping,thanks for reply!
The dts is :
/include/ "p4080ds.dts"
/ {
bp7: buffer-pool@7 {
compatible = "fsl,p4080-bpool", "fsl,bpool";
fsl,bpid = <7>;
fsl,bpool-ethernet-cfg = <0 0 0 192 0 0xdeadbeef>;
fsl,bpool-thresholds = <0x400 0xc00 0x0 0x0>;
};
bp8: buffer-pool@8 {
compatible = "fsl,p4080-bpool", "fsl,bpool";
fsl,bpid = <8>;
fsl,bpool-ethernet-cfg = <0 0 0 576 0 0xabbaf00d>;
fsl,bpool-thresholds = <0x100 0x300 0x0 0x0>;
};
bp9: buffer-pool@9 {
compatible = "fsl,p4080-bpool", "fsl,bpool";
fsl,bpid = <9>;
fsl,bpool-ethernet-cfg = <0 0 0 1728 0 0xfeedabba>;
fsl,bpool-thresholds = <0x100 0x300 0x0 0x0>;
};
bp16: buffer-pool@16 {
compatible = "fsl,p4080-bpool", "fsl,bpool";
fsl,bpid = <16>;
fsl,bpool-ethernet-cfg = <0 2048 0 1728 0 0>;
fsl,bpool-thresholds = <0x100 0x300 0x0 0x0>;
};
bp17: buffer-pool@17 {
compatible = "fsl,p4080-bpool", "fsl,bpool";
fsl,bpid = <17>;
fsl,bpool-ethernet-cfg = <0 2048 0 1728 0 0>;
fsl,bpool-thresholds = <0x100 0x300 0x0 0x0>;
};
fsl,dpaa {
ethernet@0 {
compatible = "fsl,p4080-dpa-ethernet-init", "fsl,dpa-ethernet-init";
fsl,bman-buffer-pools = <&bp7 &bp8 &bp9>;
fsl,qman-frame-queues-rx = <0x50 1 0x51 1>;
fsl,qman-frame-queues-tx = <0x70 1 0x71 1>;
};
ethernet@1{
compatible = "fsl,p4080-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet1>;
};
ethernet@2 {
compatible = "fsl,p4080-dpa-ethernet-shared", "fsl,dpa-ethernet-shared";
fsl,bman-buffer-pools = <&bp16>;
fsl,qman-frame-queues-rx = <0x54 1 0x55 1 0x4000 3>;
fsl,qman-frame-queues-tx = <0 1 0 1 0x5000 8>;
};
ethernet@3 {
compatible = "fsl,p4080-dpa-ethernet-init", "fsl,dpa-ethernet-init";
fsl,bman-buffer-pools = <&bp7 &bp8 &bp9>;
fsl,qman-frame-queues-rx = <0x56 1 0x57 1>;
fsl,qman-frame-queues-tx = <0x76 1 0x77 1>;
};
ethernet@4 {
compatible = "fsl,p4080-dpa-ethernet-init", "fsl,dpa-ethernet-init";
fsl,bman-buffer-pools = <&bp7 &bp8 &bp9>;
fsl,qman-frame-queues-rx = <0x5a 1 0x5b 1>;
fsl,qman-frame-queues-tx = <0x7a 1 0x7b 1>;
};
ethernet@5 {
compatible = "fsl,p4080-dpa-ethernet-init", "fsl,dpa-ethernet-init";
fsl,bman-buffer-pools = <&bp7 &bp8 &bp9>;
fsl,qman-frame-queues-rx = <0x5c 1 0x5d 1>;
fsl,qman-frame-queues-tx = <0x7c 1 0x7d 1>;
};
ethernet@6 {
compatible = "fsl,p4080-dpa-ethernet-init", "fsl,dpa-ethernet-init";
fsl,bman-buffer-pools = <&bp7 &bp8 &bp9>;
fsl,qman-frame-queues-rx = <0x5e 1 0x5f 1>;
fsl,qman-frame-queues-tx = <0x7e 1 0x7f 1>;
};
ethernet@7 {
compatible = "fsl,p4080-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet7>;
};
ethernet@8 {
compatible = "fsl,p4080-dpa-ethernet-shared", "fsl,dpa-ethernet-shared";
fsl,bman-buffer-pools = <&bp17>;
fsl,qman-frame-queues-rx = <0x62 1 0x63 1 0x6000 3>;
fsl,qman-frame-queues-tx = <0 1 0 1 0x7000 8>;
};
/* ethernet@9 declared as shared MAC. USDPAA will seed buffers to
* this buffer pool. The ethernet driver will initialize the RX default,
* RX error, TX error, TX confirm and 8 TX Frame queues. On receiving frame
* at this interface, the ethernet driver will do kmap_atomic/kunmap_atomic
* for that frame. */
ethernet@9 {
compatible = "fsl,p4080-dpa-ethernet-shared", "fsl,dpa-ethernet-shared";
fsl,bman-buffer-pools = <&bp17>;
fsl,qman-frame-queues-rx = <0x66 1 0x67 1 0x2000 3>;
fsl,qman-frame-queues-tx = <0 1 0 1 0x3000 8>;
};
};
};
Hello Feifei,
Please modify ethernet@9 definition to use other buffer pool rather than &bp17, because buffer pool &bp17 has already been assigned to ethernet@8.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,Yiping,thank you for your reply!
Actually in RCW the ethernet@9 is disabled,and I only enable 3 ethernet ports:ethernet@2 ethernet@7 ethernet@8,so need I to change other buffer pool for ethernet@9?
Hello Feifei,
In your original description, you pass the serdes 0xe configuration file to fmc, it seems that this is not coincident with your current target configuration.
Would you please also provide u-boot and Kernel log? It's better to include steps to setup lpm_ipfwd_app.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,Yiping,I have found the problem.In lpm-ipfwd demo,I Modified the code which didnt free the memory,so the buffer pool was always decreasing.
So thank you very much for your guidance!
Hi,Yiping,thank you for your reply!
My original description shows that the command is :lpm_ipfwd_app 1..7 -c usdpaa_config_p4_serdes_0xe.xml -p usdpaa_policy_hash_ipv4_arp_coarse_classify.xml -d 0x10000000 -b 1600:1600:1600 -n.
I rewrote a configuration file on the basis of the file usdpaa_config_p4_serdes_0xe.xml,but the contents inside has nothing to do with the usdpaa_config_p4_serdes_0xe.xml.
The contents inside the usdpaa_config_p4_serdes_0xe.xml is that:
<cfgdata>
<config>
<engine name="fm0">
<port type="1G" number="2" policy="hash_ipsec_src_dst_spi_policy0"/>
</engine>
<engine name="fm1">
<port type="1G" number="3" policy="hash_ipsec_src_dst_spi_policy1"/>
</engine>
</config>
</cfgdata>
And the u-boot and Kernel log is that:
U-Boot 2014.01QorIQ-SDK-V1.6+gfe1d4f5 (Dec 11 2015 - 16:12:47)
CPU0: P4080E, Version: 3.0, (0x82080030)
Core: e500mc, Version: 3.1, (0x80230031)
Clock Configuration:
CPU0:1199.988 MHz, CPU1:1199.988 MHz, CPU2:1199.988 MHz, CPU3:1199.988 MHz,
CPU4:1199.988 MHz, CPU5:1199.988 MHz, CPU6:1199.988 MHz, CPU7:1199.988 MHz,
CCB:599.994 MHz,
DDR:599.994 MHz (1199.988 MT/s data rate) (Asynchronous), LBC:74.999 MHz
FMAN1: 449.996 MHz
FMAN2: 449.996 MHz
QMAN: 299.997 MHz
PME: 449.996 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 4c580000 00000000 18185218 00000000
00000010: 58400000 c0002000 fe800000 e1000000
00000020: 00000000 00000000 00000000 009f8000
00000030: 20000000 00000000 00000000 00000000
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x05, vBank: 0
SERDES Reference Clocks: Bank1=125MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM TS256MSK72V3N
Detected UDIMM TS256MSK72V3N
Not enough bank(chip-select) for CS0+CS1 on controller 0, interleaving disabled!
Not enough bank(chip-select) for CS0+CS1 on controller 1, interleaving disabled!
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=8, ECC on)
DDR Controller Interleaving Mode: cache line
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KiB enabled
Corenet Platform Cache: 2 MiB enabled
Warning: SERDES8 requires banks two and three to be disabled in the RCW
SRIO1: enabled but port error
SRIO2: enabled but port error
MMC: FSL_SDHC: 0
EEPROM: Read failed.
PCIe1: disabled
PCIe2: disabled
PCIe3: disabled
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.2.14
Fman2: Uploading microcode version 106.2.14
FM1@DTSEC2, FM1@DTSEC3, FM2@DTSEC3 [PRIME], FM2@DTSEC4
Hit any key to stop autoboot: 0
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at e8020000 ...
Image Name: Linux-3.12.19-rt30-QorIQ-SDK-V1.
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 4253838 Bytes = 4.1 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at e8800000
Booting using the fdt blob at 0xe8800000
Uncompressing Kernel Image ... OK
Loading Device Tree to 03fe2000, end 03fff7cb ... OK
Using CoreNet Generic machine description
Memory CAM mapping: 256/256/256 Mb, residual: 3328Mb
Linux version 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a (freescale@freescale-sdk) (gcc version 4.8.1 (GCC) ) #4 SMP Wed Dec 23 17:10:58 CST 2015
No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(0000000000400000)
No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(0000000002000000)
Qman ver:0a01,01,02,00
No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(0000000001000000)
Bman ver:0a02,01,00
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using memblock_alloc(0x0000000001000000)
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using memblock_alloc(0x0000000000a00000)
USDPAA region at 10000000:10000000(10000:10000), 1 TLB1 entries)
CPU maps initialized for 1 thread per core
bootconsole [udbg0] enabled
setup_arch: bootmem
CoreNet Generic board from Freescale Semiconductor
arch: exit
Zone ranges:
DMA [mem 0x00000000-0x2fffffff]
Normal empty
HighMem [mem 0x30000000-0xffffffff]
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x00000000-0xffffffff]
MMU: Allocated 1088 bytes of context maps for 255 contexts
PERCPU: Embedded 8 pages/cpu @c2959000 s9792 r8192 d14784 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1047040
Kernel command line: root=/dev/mmcblk0p1 rootfstype=ext2 rootdelay=3 console=ttyS0,115200 usdpaa_mem=256M bportals=s0-1 qportals=s0-1
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Sorting __ex_table...
Memory: 3742456K/4194304K available (6640K kernel code, 336K rwdata, 1772K rodata, 272K init, 452K bss, 451848K reserved, 3407860K highmem)
Kernel virtual memory layout:
* 0xfff5f000..0xfffff000 : fixmap
* 0xffc00000..0xffe00000 : highmem PTEs
* 0xffbfa000..0xffc00000 : early ioremap
* 0xf1000000..0xffbfa000 : vmalloc & ioremap
Hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs
mpic: ISU size: 512, shift: 9, mask: 1ff
mpic: Initializing for 512 sources
clocksource: timebase mult[1aaabc25] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
mpic: requesting IPIs...
e500 family performance monitor hardware support registered
Brought up 8 CPUs
devtmpfs: initialized
NET: Registered protocol family 16
PCI: Probing PCI hardware
Setting up RapidIO peer-to-peer network /rapidio@ffe0c0000
fsl-of-rio ffe0c0000.rapidio: Of-device full name /rapidio@ffe0c0000
fsl-of-rio ffe0c0000.rapidio: Regs: [mem 0xffe0c0000-0xffe0d0fff]
fsl-of-rio ffe0c0000.rapidio: bellirq: 57
fsl-of-rio ffe0c0000.rapidio: pwirq: 478
fsl-of-rio ffe0c0000.rapidio: /rapidio@ffe0c0000/port1: LAW start 0x0000000c20000000, size 0x0000000010000000.
fsl-of-rio ffe0c0000.rapidio: RapidIO PHY type: Serial
fsl-of-rio ffe0c0000.rapidio: Port 0 is not ready. Try to restart connection...
fsl-of-rio ffe0c0000.rapidio: Port 0 restart failed.
fsl-of-rio ffe0c0000.rapidio: /rapidio@ffe0c0000/port2: LAW start 0x0000000c30000000, size 0x0000000010000000.
fsl-of-rio ffe0c0000.rapidio: RapidIO PHY type: Serial
fsl-of-rio ffe0c0000.rapidio: Port 1 is not ready. Try to restart connection...
fsl-of-rio ffe0c0000.rapidio: Port 1 restart failed.
fsl-of-rio: probe of ffe0c0000.rapidio failed with error -67
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
EDAC MC: Ver: 3.0.0
Bman err interrupt handler present
Bman portal (shared) initialised, cpu 0
Bman portal (shared) initialised, cpu 1
Bman portal (slave) initialised, cpu 2
Bman portal (slave) initialised, cpu 3
Bman portal (slave) initialised, cpu 4
Bman portal (slave) initialised, cpu 5
Bman portal (slave) initialised, cpu 6
Bman portal (slave) initialised, cpu 7
Bman portals initialised
Qman err interrupt handler present
Qman portal (shared) initialised, cpu 0
Qman portal (shared) initialised, cpu 1
Qman portal (slave) initialised, cpu 2
Qman portal (slave) initialised, cpu 3
Qman portal (slave) initialised, cpu 4
Qman portal (slave) initialised, cpu 5
Qman portal (slave) initialised, cpu 6
Qman portal (slave) initialised, cpu 7
Qman portals initialised
Bman: BPID allocator includes range 32:32
Qman: FQID allocator includes range 256:256
Qman: FQID allocator includes range 32768:32768
Qman: CGRID allocator includes range 0:256
Qman: pool channel allocator includes range 33:15
Switched to clocksource timebase
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
audit: initializing netlink socket (disabled)
type=2000 audit(0.519:1): initialized
bounce pool size: 64 pages
HugeTLB registered 1 MB page size, pre-allocated 0 pages
HugeTLB registered 4 MB page size, pre-allocated 0 pages
HugeTLB registered 16 MB page size, pre-allocated 0 pages
HugeTLB registered 64 MB page size, pre-allocated 0 pages
HugeTLB registered 256 MB page size, pre-allocated 0 pages
HugeTLB registered 1 GB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
NTFS driver 2.1.30 [Flags: R/O].
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 782
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 18749812) is a 16550A
console [ttyS0] enabled, bootconsole disabled
console [ttyS0] enabled, bootconsole disabled
serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 18749812) is a 16550A
serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 18749812) is a 16550A
serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 18749812) is a 16550A
ePAPR hypervisor byte channel driver
Generic non-volatile memory driver v1.1
brd: module loaded
loop: module loaded
st: Version 20101219, fixed bufsize 32768, s/g segs 256
fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000001 Chip ID 0x002801
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.5.
number of CFI chips: 1
fsl_espi ffe110000.spi: master is unqueued, this is deprecated
m25p80 spi32766.0: unrecognized JEDEC id 80900c
fsl_espi ffe110000.spi: at 0xf115e000 (irq = 53)
libphy: Fixed MDIO Bus: probed
platform mdio-mux-emi1.14: Driver mdio-mux-gpio requests probe deferral
platform mdio-mux-emi2.15: Driver mdio-mux-gpio requests probe deferral
libphy: Freescale PowerQUICC MII Bus: probed
mdio_bus mdio@ffe4e1120: cannot get PHY at address 8
libphy: Freescale XGMAC MDIO Bus: probed
Freescale FM module (Dec 23 2015:09:02:25), FMD API version 21.1.0
Freescale FM Ports module (Dec 23 2015:09:02:26)
dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()
dpaa_generic_debugfs: FSL DPAA Ethernet debugfs entries ()
fsl_mac: fsl_mac: FSL FMan MAC API based driver ()
fsl_mac ffe4e0000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:0c:bd:00:d0:97
fsl_mac ffe4e2000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:0c:bd:00:d0:88
fsl_mac ffe4e4000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:0c:bd:00:d0:89
fsl_mac ffe5e4000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe5e4000.ethernet: FMan MAC address: 00:0c:bd:00:d9:94
fsl_mac ffe5e6000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe5e6000.ethernet: FMan MAC address: 00:0c:bd:00:d0:95
fsl_dpa: FSL DPAA Ethernet driver ()
fsl_dpa: fsl_dpa: Probed interface eth0
fsl_dpa_shared: FSL DPAA Shared Ethernet driver ()
fsl_dpa_shared: fsl_dpa_shared: Probed shared interface eth1
fsl_dpa_shared: fsl_dpa_shared: Probed shared interface eth2
fsl_dpa_shared: fsl_dpa_shared: Probed shared interface eth3
fsl_dpa_proxy: FSL DPAA Proxy initialization driver ()
fsl_oh: FSL FMan Offline Parsing port driver ()
fsl_oh dpa-fman0-oh.21: Found OH node handle compatible with fsl,dpa-oh.
fsl_oh dpa-fman0-oh.21: Allocating 0 ingress frame queues duples
fsl_oh dpa-fman0-oh.21: OH port /soc@ffe000000/fman@400000/port@82000 has no buffer pool. Fragmentation will not be enabled
fsl_oh dpa-fman0-oh.21: OH port /soc@ffe000000/fman@400000/port@82000 enabled.
fsl_oh dpa-fman0-oh.21: Default egress frame queue: 105
fsl_oh dpa-fman0-oh.21: Default error frame queue: 104
fsl_oh dpa-fman0-oh.21: Initialized queues:
e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
e1000: Copyright (c) 1999-2006 Intel Corporation.
e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
e1000e: Copyright(c) 1999 - 2013 Intel Corporation.
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci-pci: OHCI PCI platform driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver usb-storage
ampc-i2c ffe118000.i2c: timeout 1000000 us
mpc-i2c ffe118100.i2c: timeout 1000000 us
mpc-i2c ffe119000.i2c: timeout 1000000 us
mpc-i2c ffe119100.i2c: timeout 1000000 us
at24 4-0050: 65536 byte 24c512 EEPROM, writable, 1 bytes/write
rtc-ds3232 4-0068: rtc core: registered ds3232 as rtc0
i2c i2c-0: Added multiplexed i2c bus 4
i2c i2c-0: Added multiplexed i2c bus 5
i2c i2c-0: Added multiplexed i2c bus 6
i2c i2c-0: Added multiplexed i2c bus 7
i2c i2c-0: Added multiplexed i2c bus 8
i2c i2c-0: Added multiplexed i2c bus 9
i2c i2c-0: Added multiplexed i2c bus 10
i2c i2c-0: Added multiplexed i2c bus 11
pca954x 0-0077: registered 8 multiplexed busses for I2C mux pca9547
Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software
EDAC MC0: Giving out device to 'MPC85xx_edac' 'mpc85xx_mc_err': DEV mpc85xx_mc_err
MPC85xx_edac acquired irq 490 for MC
MPC85xx_edac MC err registered
EDAC MC1: Giving out device to 'MPC85xx_edac' 'mpc85xx_mc_err': DEV mpc85xx_mc_err
MPC85xx_edac acquired irq 489 for MC
MPC85xx_edac MC err registered
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using DMA
platform caam_qi.0: Linux CAAM Queue I/F driver initialised
caam ffe300000.crypto: device ID = 0x0a10030000000000 (Era 4)
caam ffe300000.crypto: job rings = 4, qi = 1
caam algorithms registered in /proc/crypto
caam_jr ffe301000.jr: registering rng-caam
mmc0: new high speed SDHC card at address 0007
caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto
platform caam_qi.0: fsl,sec-v4.0 algorithms registered in /proc/crypto
Freescale USDPAA process driver
Freescale USDPAA process IRQ driver
fsl-pme ffe316000.pme: ver: 0x00100201
Freescale pme2 db driver
mmcblk0: mmc0:0007 SQFSD 7.42 GiB
mmcblk0: p1
Freescale pme2 scan driver
fsl-pme2-scan: device pme_scan registered
Freescale hypervisor management driver
fsl-hv: no hypervisor found
ipip: IPv4 over IPv4 tunneling driver
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
libphy: mdio_mux: probed
libphy: mdio_mux: probed
mdio_bus 0.1: cannot get PHY at address 28
mdio_bus 0.1: cannot get PHY at address 29
libphy: mdio_mux: probed
mdio_bus 0.3: cannot get PHY at address 28
mdio_bus 0.3: cannot get PHY at address 29
mdio_bus 0.3: cannot get PHY at address 30
mdio-mux-gpio mdio-mux-emi1.14: Version 1.0
fsl_dpa_macless: FSL DPAA MACless Ethernet driver ()
fsl_dpa_generic: FSL DPAA Generic Ethernet driver ()
rtc-ds3232 4-0068: setting system clock to 2016-01-16 09:45:24 UTC (1452937524)
Waiting 3 sec before mounting root device...
VFS: Mounted root (ext2 filesystem) readonly on device 179:1.
devtmpfs: mounted
Freeing unused kernel memory: 272K (c083b000 - c087f000)
INIT: version 2.88 booting
/etc/init.d/rcS: line 27: /etc/hostname: Read-only file system
Starting udev
udevd[1074]: starting version 182
EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
net.ipv4.conf.default.rp_filter = 0
net.ipv4.conf.all.rp_filter = 0
Starting atd: OK
INIT: Entering runlevel: 5
Configuring network interfaces... done.
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting rpcbind daemon...done.
creating NFS state directory: done
starting statd: done
Starting network benchmark server: netserver.
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
starting 8 nfsd kernel threads: done
starting mountd: done
Starting system log daemon...0
Starting kernel log daemon...0
Starting internet superserver: xinetd.
Starting crond: OK
Starting MySQL.[ OK ]
Stopping Bootlog daemon: bootlogd.
Starting tcf-agent: OK
Welcome to FEC! p4080ds Saturday, 16 January 2016 09:45:30
p4080ds login: root
Today the problem happened again,and I checked that the buffer pool for fm2-gb3 which was connected to Internet has no buffers:
# cat /sys/devices/ffe000000.soc/ffe31a000.bman/pool_count/17
0
But the buffer pool for fm1-gb2 which was not connected to Internet has many buffers
# cat /sys/devices/ffe000000.soc/ffe31a000.bman/pool_count/16
1600
So how do I solve the problem? Thank you !