About the power measurement device of p2020.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the power measurement device of p2020.

1,468 Views
minjokim
Contributor I

Hi, All.

I have a question.

I use the p2020rdb board and I want to measure the power consumption of p2020.

So, I searched about the some power measurement device (power meter?)

including the software that can analyze the power consumption of p2020.

     1. Monsoon power monitor (Monsoon Solutions) -> only mobile device??

     2. Yokogawa wt310 (Value Series Power Analyzer WT300 - Digital Power Analyzers - Power Analyzers - Yokogawa)

Can I utilize above two devices to measure the power consumption of p2020rdb ??

If so, which one is more proper? (easily using)

Thanks in advance. :smileyhappy:

Minjo.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,204 Views
alexander_yakov
NXP Employee
NXP Employee

Usually, power measurement is done by measuring the current the device consumes, and than multiplying this value to the power supply voltage.

Another way (usually used when designing power supply) is to look P2020 device datasheet for approximate power numbers.

I do not think we have experience with these specific power measurement tools

0 Kudos
Reply