How to use "FLASH NOUNSECURE" in CW10.7?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use "FLASH NOUNSECURE" in CW10.7?

522 次查看
wangjiajie
Contributor III

I hane write a bootloader and a application according to AN4258 ,i created both project in CW 10.7, there is a note in AN4258 to merge the two project, but in CW10.7 i can not find these:

6. Add the following command into the file ..\user_application_project\cmd\P&E_Multilink_CyclonePro_Preload.cmd:
FLASH NOUNSECURE

20171018170210119.jpg

0 项奖励
1 回复

309 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Wang,

There is difference between CW5.1 and CW10.7, please refer to

https://community.nxp.com/docs/DOC-335384 

this is for S12Z cw10.7 .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励