I hane write a bootloader and a application according to AN4258 ,i created both project in CW 10.7, there is a note in AN4258 to merge the two project, but in CW10.7 i can not find these:
6. Add the following command into the file ..\user_application_project\cmd\P&E_Multilink_CyclonePro_Preload.cmd:
FLASH NOUNSECURE
Hello Wang,
There is difference between CW5.1 and CW10.7, please refer to
https://community.nxp.com/docs/DOC-335384
this is for S12Z cw10.7 .
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------