max votlage on TEA2208

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

max votlage on TEA2208

1,195件の閲覧回数
febat
Contributor I

Dear All,

for a new project of a power supply at 30Vcc and up 15A, I'm evaluation to use TEA2208 as active full-bridge controller.

The archietecture is very simple:
1) toroidal transformer from 230Vac to 31Vac (tolerance -15% / +10%)
2) bridge
3) dc-dc to have 30Vcc.

So I would like to use the TEA2208 as ative full bridge contoller, but I think it's not possible because Vcc max voltage il 14V, instead in my project the Vout is 31Vcc...

Solutions?

Thank You and Best Regards
Federico Battaglin

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,066件の閲覧回数
femartech
Contributor I

I don't understand what means Vth...

I noted VL and VR is hundreds Volt... but I can't have the DC Vout about 32V... it's very strange...

Someone clarify me...

Best Regards
Federico

 

0 件の賞賛
返信

1,162件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Perhaps you misunderstand this VCC define which is no problem for your case ,but  you should consider about the VTH max is 32V but in your application is 31V.

guoweisun_1-1689050780718.png

 

guoweisun_0-1689050745899.png

 

0 件の賞賛
返信