max votlage on TEA2208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

max votlage on TEA2208

1,052 Views
febat
Contributor I

Dear All,

for a new project of a power supply at 30Vcc and up 15A, I'm evaluation to use TEA2208 as active full-bridge controller.

The archietecture is very simple:
1) toroidal transformer from 230Vac to 31Vac (tolerance -15% / +10%)
2) bridge
3) dc-dc to have 30Vcc.

So I would like to use the TEA2208 as ative full bridge contoller, but I think it's not possible because Vcc max voltage il 14V, instead in my project the Vout is 31Vcc...

Solutions?

Thank You and Best Regards
Federico Battaglin

 

Labels (1)
0 Kudos
Reply
2 Replies

923 Views
femartech
Contributor I

I don't understand what means Vth...

I noted VL and VR is hundreds Volt... but I can't have the DC Vout about 32V... it's very strange...

Someone clarify me...

Best Regards
Federico

 

0 Kudos
Reply

1,019 Views
guoweisun
NXP TechSupport
NXP TechSupport

Perhaps you misunderstand this VCC define which is no problem for your case ,but  you should consider about the VTH max is 32V but in your application is 31V.

guoweisun_1-1689050780718.png

 

guoweisun_0-1689050745899.png

 

0 Kudos
Reply