Datasheet says "12.2.1.1 Mode 1 (manual mode)
The DC-to-DC converter control mode 1 is chosen by microcode and is set as the
default. The current_feedback_4 is monitored by microcode and the LS7 is controlled
completely via microcode. The low side is controlled directly by the microcore using the
'sto' instruction."
I can find no example.
Has anyone tried this, as "12.2.1.2 Mode2 (hysteretic control)" generates too fast LS7 at over 2MHz!