GD3160 watchdog fault (WDOG_FLT) cannot be cleared

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GD3160 watchdog fault (WDOG_FLT) cannot be cleared

1,963 Views
bkreger
Contributor III
We are working on a project that uses six (6) GD3160 ICs and are currently working to get the devices initialized and configured. Specifically, we have implemented the power-up sequence provided in the Data Sheet (rev 11.0).

After powering the high-voltage domain (step 4a), and attempting to clear faults, the watchdog faults remain enabled (the watchdog fault is asserted on all 6 GD3160s).  A check of power supply voltages show that these are within acceptable ranges (we do not get faults for VSUP, VDD, VCC, or VREF either).

The data sheet says the following:  "A watchdog fault will latch when VSUP, VDD, VCC, or VREF falls below POR threshold voltage levels and exceeds the programmable watchdog timeout duration."  Are there any other conditions which would cause a watchdog fault to occur?
Labels (1)
0 Kudos
Reply
4 Replies

1,922 Views
guoweisun
NXP TechSupport
NXP TechSupport

If CSB signal is low for a longer period than Watchdog time out, a watchdog fault

(WDOG_FLT) will be reported.

0 Kudos
Reply

1,886 Views
bkreger
Contributor III

Thanks for the quick response to my question.  I have some additional data for this issue.

Attached is a logic analyzer screen capture of the SPI communication to the GD3160s (in GD3160-SPI-Chain-Signals.png).  It shows that for a transmit to the three-device chain the chip select is active (low) for 9.4 us.  We checked this for multiple transmits and verified that it does not deviate much from this value (10s of ns).

Also, we have measured the voltages on the GD3160 voltage supply rails. They all look stable as shown in the attached file (pdf below).

Any thoughts on what the cause could be?

Thank you.

0 Kudos
Reply

1,962 Views
bkreger
Contributor III
Further information:
INTA is high
INTB is low
PWM signals are all low
FSENB is high
0 Kudos
Reply

1,867 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the power up sequency, you can try to power on high voltage firstly then next power on the low voltage for GN3160.

0 Kudos
Reply