mpc8349 mitx cant erase or progrmam flash with CW.
using EN29LV640H:
message
Error: Getting flash ID failed
this is the log:
: -------------------------
Using Algorithm: amd16x1.elf
======================================================================
=== Target Configuration Settings
=== Connection: CodeWarrior USB TAP
=== Target Processor: 8349
=== Target Init File: C:\Users\ali\Desktop\MPC8349E\mpc8349e-mitx-20070221\CW Files\8349ITX_init.cfg
======================================================================
Connecting......Connected
======================================================================
=== Execute: Erase
=== Timestamp: Mon May 4 19:28:41 2015
=== Flash Device: MX29LV640MTTC
=== Flash Organization: 4Mx16x1
=== Flash Mem Start Addr: 0xFE000000
=== Flash Mem End Addr: 0xFE7FFFFF
======================================================================
Informing other connection clients that the target is being 'clobbered'.
Loading Flash Device Driver at: 0x00000000
Flash Driver Buffer is at: 0x00001E00
Flash Driver Buffer Size is: 0x00104200
Flash Programmer: Flash driver reports the following error(s):
Timestamp: Mon May 4 19:28:43 2015