Hi,
I have been configuring HDLC controller for MPC8309TWR freescale board,but event register UCCE shows line is busy that's why frames are discarded due to lack of buffers.Actually my TX is working fine.
So please suggest what can be done for buffer handling.
Thanks
Muazzam(india)
已解决! 转到解答。
"Busy" means the current Rx buffer descriptor (RxBD), prefetched from RxBD table for data reception, is not empty - RxBD[E] bit is cleared.
The following is said in QE Reference Manual, Section 14.3.2: "If a match is detected, the HDLC controller checks the prefetched BD, and if empty, begins transferring the incoming frame to the BD’s associated buffer." So, if this buffer is not empty, "busy" condition occurs.
HDLC parameter ram, parameter "RBPTR" points to the current RxBD during frame reception. At the initialization, this parameter is equal to "RBASE", i.e. point to the first entry in RxBD table.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
"Busy" means the current Rx buffer descriptor (RxBD), prefetched from RxBD table for data reception, is not empty - RxBD[E] bit is cleared.
The following is said in QE Reference Manual, Section 14.3.2: "If a match is detected, the HDLC controller checks the prefetched BD, and if empty, begins transferring the incoming frame to the BD’s associated buffer." So, if this buffer is not empty, "busy" condition occurs.
HDLC parameter ram, parameter "RBPTR" points to the current RxBD during frame reception. At the initialization, this parameter is equal to "RBASE", i.e. point to the first entry in RxBD table.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok, run the controller, wait until the problem appears, than stop the controller by clearing ENT and ENR bits in GUMR_L register. Please do not modify anything except GUMR_L[ENT, ENR] bits. After that, please dump all UCC-related registers, parameter ram and buffer descriptors tables. Please submit me this dump for analysis.
hi ,
Thanks for your all effort for helping me ,i got RX too. Actually i had to assign RXBD base addr to rbptr,I was actually assigning to just rbase not rbptr.so Now it's working .
Thanks :smileyhappy:
Muazzam(india)