location of pcie AC-couple cap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

location of pcie AC-couple cap

999件の閲覧回数
lu_chunjie23
Contributor I

For T1040 (PCIe Gen 2.0 run @5Gbps) , if the  PCIe Tx&Rx chips are on same pcb, could the ac-coulpe caps of PCIe link be placed on the Rx side?

Will the eye pattern be better than the caps placed on Tx side?

タグ(1)
0 件の賞賛
1 返信

726件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

The serdes can operates when the AC-coulpe caps of link are placed on the Rx side. For example AC coupling caps for SGMII are placed near the receiver inputs (standard). So if PCIe Tx&Rx chips are fixed on the same pcb, the ac-coulpe caps of PCIe link can be placed on the Rx side. I do not see why the eye pattern be better in this case. You should ensure by simulation that the Rx data eyes at each link partner’s receiver is in spec in both cases.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛