MPC8347E AVDD Current details

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8347E AVDD Current details

663 次查看
dhoresh_adabala
Contributor I

Hello for MPC8347E there are AVDD1 to AVDD4 pins (PLL supply voltage) with supply voltage of 1.2V. What is the current requirement for these power input pins? There is no mention of the supply current requirement for AVDD supply across the datasheet. Please provide supply current requirements for AVDD Pins of MPC8347E. 

0 项奖励
回复
1 回复

592 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

AVdd power is negligibly small comparing to the core. Peak PLL current is not greater than 5mA for each AVdd power supply.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复