Unable to communicate with an RMII Ethernet Switch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to communicate with an RMII Ethernet Switch

2,252件の閲覧回数
hilairenicolas
Contributor I

We're currently triying to communicate using RMII bus with a Micrel Ethernet Switch (KZS8895RQ).

We also using MDC / MDIO link to configure it.

The MDC / MDIO link works well. We can see when a connection is established on a port of the switch.

We have plugged the RMII of our MPC8377 to the SW5 MAC of the Switch.

We have configured the MAC of the Switch to work in "PHY Mode" to permit to communicate with the MAC of our MPC8377.

We have successfully configured the MPC8377 to work in RMII mode and not in RGMII (default value)

We have made this connection:

cablage.png

The clock is generated at 50MHz by the Switch.

We are in Linux 2.6.38  Environment with an adapted generic driver from micrel.c file.

We are using dts to configure our switch :

mdio@24520 {

  #address-cells = <1>;

  #size-cells = <0>;

  compatible = "fsl,gianfar-mdio";

  reg = <0x24520 0x20>;

  ksz8895_1: ethernet-phy@1 {

  interrupt-parent = <&ipic>;

  reg = <0x1>;

  device_type = "ethernet-phy";

  };

   };

enet0: ethernet@25000 {

  #address-cells = <1>;

  #size-cells = <1>;

  cell-index = <0>;

  device_type = "network";

  model = "eTSEC";

  compatible = "gianfar";

  reg = <0x25000 0x1000>;

  ranges = <0x0 0x25000 0x1000>;

  local-mac-address = [ 12 23 45 56 67 01 ];

  interrupts = <35 0x8 36 0x8 37 0x8>;

  phy-connection-type = "rmii";

  interrupt-parent = <&ipic>;

  phy-handle = <&ksz8895_1>;

  sleep = <&pmc 0xc0000000>;

  fsl,magic-packet;

  };

When we make ping from the linux board to a PC connected to the switch we can see data on the RMII bus with a scope but never on the Ethernet

When we make a ping from the PC to the board, wa can see RMII data but linux never see them.

When we plug two computer onto the switch they communicate successfully (so the ethernet transformer are Ok)

Why ?

Any idea ? or question to clarify my request ?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

997件の閲覧回数
sinanakman
Senior Contributor III

Hi Nicolas

>  local-mac-address = [ 12 23 45 56 67 01 ];

Please don't do this. This may or may not be the source

of the problem but please only use a valid mac address.

If you don't know the mac address of your phy you can

generate a temporary (fake) one with tools/gen_eth_addr

from mainline uboot sources (e.g. here is one I

generated now for you : 1a:2b:6a:60:89:02)

Hope this helps

Sinan Akman

0 件の賞賛
返信

997件の閲覧回数
hilairenicolas
Contributor I

ok thank you, I will use this mac address But effectively, it doesn't correct the problem. :smileysad:

0 件の賞賛
返信