Segger J-Link with LS1046A Freeway

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Segger J-Link with LS1046A Freeway

Jump to solution
2,032 Views
jekim
Contributor IV

Hello,

I installed CodeWarrior Studio 11.5.2. I'm trying to add new connection for LS1046A Freeway. It seems the probe type is fixed to CWTAP. Is it possible to add segger J-Link in the connection? Thanks.

Best Regards,

Jeff

0 Kudos
Reply
1 Solution
2,028 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> Is it possible to add segger J-Link in the connection?

This is not possible.

View solution in original post

3 Replies
2,029 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> Is it possible to add segger J-Link in the connection?

This is not possible.

2,018 Views
jekim
Contributor IV

Dear Fedor,

 

Thank you for the confirmation. Then, below base unit and tip are enough for LS1046A Freeway debug?

CWH-CTP-CTX10-YE Product Information|NXP

CWH-CTP-BASE-HE Product Information|NXP

 

Best Regards,

Jeff

0 Kudos
Reply
2,011 Views
ufedor
NXP Employee
NXP Employee

Yes, these are correct TAP and Probe Tip for ARM processors.

0 Kudos
Reply