We are having a customised board with P1022 processor, we are booting the uboot via spi flash. kernel, dtb , fs are booted using nand flash. We are facing issue in booting the linux from nand flash and kernel throws exception continuously. Nand flash is connected on local bus with P1022 processor.
Part number of nand flash Micron MT29F4G08ABADAWP.
The logs of the same is attached in the file.
已解决! 转到解答。
Is there similar problem if SPI is used for booting the kernel, rootfs and .dtb file? There is message in your log that there are bad blocks in your NAND. Test NAND Flash writing/reading under u-boot.
Is there similar problem if SPI is used for booting the kernel, rootfs and .dtb file? There is message in your log that there are bad blocks in your NAND. Test NAND Flash writing/reading under u-boot.
@PavelWe will work on the two solution provided by you.
Meanwhile line number 264 in the attached logs
talitos ffe30000.crypto: failed to register hwrng: -19
This error seems to be only difference between working kernel in some other board and this board. Can you throw some light regarding this error?