My router has 8GB DDR what config need to change in UBOOT to access 8GB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

My router has 8GB DDR what config need to change in UBOOT to access 8GB

1,807 Views
ramakrishnakatt
Contributor II

we are using powerpc-fsl_networking-linux-gcc? is this sufficient or we need to use 64bit power pc compiler.

Labels (1)
0 Kudos
Reply
6 Replies

1,442 Views
LPP
NXP Employee
NXP Employee

36-bit address mode is required to support physical memory larger than 4GB

Please refer to Section 6.1.3 U-boot Configuration of the following document:

Freescale Linux SDK for QorIQ Processors

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.7-IC-RevB.zip

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,442 Views
ramakrishnakatt
Contributor II

Hi Pavel,

Thanks for your information, but in our current uboot code i did not find any config files with name T1040RDB_36BIT_config

Can you point out the config file for 36-bit access in Uboot

Thanks

Rama

0 Kudos
Reply

1,442 Views
scottwood
NXP Employee
NXP Employee

T1040 U-Boot always supports 36-bit addressing.  You don't need to do anything special.

0 Kudos
Reply

1,442 Views
ramakrishnakatt
Contributor II

Hi Scott,

Our requirement is to test Uboot higher address, we can't  able to access higher address from Uboot prompt.

if we want access, 0xfe0000000, from uboot prompt how we will access?

if we try to dump with md command it is displaying only 0xe0000000,, what is the solution, what things we have to change to make 36-bit access

0 Kudos
Reply

1,442 Views
scottwood
NXP Employee
NXP Employee

FWIW, 0xfe0000000 is CCSR which is mapped to virtual 0xe0000000, so you can use md for that.  You just can't access DDR above 2 GiB.

0 Kudos
Reply

1,442 Views
scottwood
NXP Employee
NXP Employee

U-Boot on PPC always runs in 32-bit mode, so it can't address that extra RAM itself.  To access it, you need to load an OS, or write a standalone application or custom U-Boot code that creates temporary TLB mappings to access it in chunks.

0 Kudos
Reply