MPC8548 when reads the data from the PCIE is and to write into the DDR2 CPU core intervention is required or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8548 when reads the data from the PCIE is and to write into the DDR2 CPU core intervention is required or not?

826 Views
lakshmit
Contributor I

PC8548 when reads the data from the PCIE is and to write into the DDR2 CPU core intervention is required or not?

0 Kudos
Reply
1 Reply

763 Views
ufedor
NXP Employee
NXP Employee

The CPU intervention is not required - i.e. PCI Express transactions targeting MPC8548 inbound ATMU with translation to a DDR2 SDRAM region are converted to direct memory read/write operations by the PCI Express interface.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply