MPC8308 's hardware question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8308 's hardware question

348 次查看
bsw_0204107
Contributor I

hi! in MPC8308, can I dirrectly use one USB without PHY?

标记 (1)
0 项奖励
1 回复

297 次查看
Pavel
NXP Employee
NXP Employee

The MPC8308 USB ULPI cannot be connected to other USB ULPI controller. The MPC8308 USB ULPI control signals are inputs: USBDR_PWR_FAULT, USBDR_CLK, USBDR_DIR and USBDR_NXT. See the Table 13-1 of the MPC8308 Reference Manual.

It required using a USB ULPI PHY.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励