MPC5606b Drives

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5606b Drives

935件の閲覧回数
利中舒
Contributor II

Where can I get MPC5606B's Drives or examples,!  Thanks very much!

0 件の賞賛
返信
1 返信

808件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

The AN2865 Cookbook gives you almost all you need for starting a work on MPC5606B. Not all peripherals are handled, but almost all.

You can find AN2865 and the demo examples from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC560xB&fpsp=1&tab=Documentation_Tab

These examples are also available as the CodeWarrior demo examples. See more in Classic CodeWarrior installation:

C:\Program Files\Freescale\CW for MPC55xx and MPC56xx 2.10\(CodeWarrior_Examples)\560xB-CW\

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信