MLC NAND Support for P1021 with SDK1.7 release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MLC NAND Support for P1021 with SDK1.7 release

ソリューションへジャンプ
1,382件の閲覧回数
shubhasingh
Contributor I

Hi,

Can anyone clarify me regarding the MLC nand driver support with the kernel 3.12 for P1021 released with SDK 1.7 QorIQ.

Thanks,

Shubha

タグ(1)
0 件の賞賛
返信
1 解決策
1,248件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello shubha singh,

For P1021, FCM does not support MLC NAND as its ECC requirement, it works if software ECC used.

And as I remember Freescale SDK does not include software BCH ECC, I'll confirm further if this is the case for 1.7.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,249件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello shubha singh,

For P1021, FCM does not support MLC NAND as its ECC requirement, it works if software ECC used.

And as I remember Freescale SDK does not include software BCH ECC, I'll confirm further if this is the case for 1.7.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,248件の閲覧回数
shubhasingh
Contributor I

Thanks, lunminliang

I am planning to add the BCH ECC support for 4 bit ECC, could you please provide me some information on this.

Regards,

Shubha

0 件の賞賛
返信