1. The main difference is that 10G AQR PHYs have been changed, PHY addresses are also changed.
Please refer to the following in LSDK 21.08 for Rev C in u-boot source code.
/* MAC/PHY configuration */
#if defined(CONFIG_FSL_MC_ENET)
#define CONFIG_MII
#define CONFIG_ETHPRIME "DPMAC1@xgmii"
#define AQR113C_PHY_ADDR1 0x0
#define AQR113C_PHY_ADDR2 0x08
Please refer to the following in LSDK 20.04 for Rev B in u-boot source code.
#define AQR107_PHY_ADDR1 0x04
#define AQR107_PHY_ADDR2 0x05
#define AQR107_IRQ_MASK 0x0C
2. For LX2160ardb Rev.C board, please use LSDK 21.08.