How to access 4GB DDR space for p2020?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to access 4GB DDR space for p2020?

1,528件の閲覧回数
982576385
Contributor I
How to access 4GB DDR space for p2020?
0 件の賞賛
返信
2 返答(返信)

1,520件の閲覧回数
Bulat
NXP Employee
NXP Employee

The P2020 is equipped with e500v2 cores, the core provides 36-bit addressing, i.e. can address 64GB of memory space. So 4GB of DDR is not a problem.

I would add that the MMU (Memory Management Unit) is responsible for translation of 32-bit accesses to 36-bit address space. Details can be found in the e500 reference manual, see section 12:

https://www.nxp.com/docs/en/reference-manual/E500CORERM.pdf

 

Regards,

Bulat

 

 

0 件の賞賛
返信

1,517件の閲覧回数
982576385
Contributor I

thanks,that is rigth.

but the effective address is 32 bit in p2020,it means that i can only use 4GB memory. where can i place other memory if i used all 4GB for ddr?

can i use on chip memory less than 4GB to access all the 4GB space of ddr simultaneously?

 

0 件の賞賛
返信